AXIS#.GEAR.DEC
Description
AXIS#GEAR.DEC defines the maximum deceleration rate the slave will follow to come out of gearing, to rest. AXIS#GEAR.DEC will only be used if Gearing is stopped for any reason, including if an AXIS#.STOP command is issued. As soon as the axis has come to rest, AXIS#GEAR.DEC will no longer be in effect and the axis will behave according to the rules of whatever motion is commanded next.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
Type |
Read/Write |
Units |
Rotary: RPM See Acceleration Units for details. |
Range |
Depends on units. See Acceleration Range for details. |
Default Value |
10,000 RPM/s Depends on units. See Acceleration Units for details. |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.GEAR.DEC | 0x5006 | 0x2 | UDINT | - | Acceleration | RW | False |
AXIS2.GEAR.DEC | 0x5106 | 0x2 | UDINT | - | Acceleration | RW | False |